Technical FAQs

Ask a Question

Can a QO342M150 load center be converted to a main lug only panel?

Issue:
Application

Product Line:
QO Load Center

Environment:
Application

Cause:
Clarification of feature

Resolution:
This is an obsolete design of convertible main breaker load center that can be converted to main lug only by removing the main circuit breaker and installing Main Lug Kit QOL3225. You will also need to add Filler Plate KFP to the main breaker opening in the covers dead-front trim.
(2/5/15 update - the KFP filler plate is now obsolete and no longer available).


CTA-ID : 2000091
Was this helpful?
What can we do to improve the information ?