Technical FAQs

Ask a Question

What components are required to add a standard capacity 480 to 120 volt control power transformer to a 8538SD or 8539SD combination starter?

Issue:
Field installation of a control power transformer

Product Line:
NEMA combination starters

Environment:
Products sold and used in the United States

Cause:
Need a transformer for 480VAC primary down to 120VAC secondary in a combination starter

Resolution:
9070T100D1 control power transformer, 9999SFR4 primary fuse holder, (2) .50 amp primary fuses (Class CC Time Delay ONLY - Use Bussman FNQR or Littlefuse KLDR). If secondary fuse is desired order 9080PF1 and 1.00 amp standard 30A 250V cartridge fuse (2`` x 9/16``).


CTA-ID : 15174
Was this helpful?
What can we do to improve the information ?