Technical FAQs

Ask a Question

How many power contacts can you field convert to normally closed on an 8903 type L electrically held?

Up to 8 contacts can be field converted to normally closed. If a contactor with more than 8 normally closed contacts is required, it may be obtained by ordering it from the factory.


CTA-ID : 2000385
Was this helpful?
What can we do to improve the information ?