Technical FAQs

Ask a Question

Do the CTs in the Proxima cradle meet this statement?<br /><br />ANSI C12.16 certified revenue accuracy metering

The CT`s were designed for C37.20.1 metering accuracy. The Proxima specification never called for revenue accuracy.


CTA-ID : 2000080
Was this helpful?
What can we do to improve the information ?