Technical FAQs

Ask a Question

What is the temperature rating on the lugs for the CK800N?

The temperature rating is 75 deg c copper wire. The breaker and lugs are tested as a system using 75 deg wire.


CTA-ID : 16018
Was this helpful?
What can we do to improve the information ?