Technical FAQs

Ask a Question

Can the QO142L225G load center be converted to a main breaker load center?

Issue:
product design features

Product Line:
QO Load centers

Environment:
Convertible to main breaker

Cause:
Application

Resolution:
Yes, the QO142L225G load center can be converted by field installing a QOM2 Frame size Main Breaker Kit. Below are the available amperages

100amp use a QOM2100VH
125amp use a QOM2125VH
150amp use a QOM2150VH
175amp use a QOM2175VH
200amp use a QOM2200VH
225amp use a QOM2225VH .


CTA-ID : 2000377
Was this helpful?
What can we do to improve the information ?