Technical FAQs

Ask a Question

Can a white LED, such as catalog number DL1BDB1, be applied with colored lens units?

It is recommended that the LED color should match the color of the lens unit. Use red LED with a red lens unit, a green LED with a green lens unit, etc.

CTA-ID : 2000365
Was this helpful?
What can we do to improve the information ?