Technical FAQs

Ask a Question

Is there a piece of MP metering mounting channel available that could be cut to any desired length in the field?<br />

There is a 6` (6 foot) piece of EZM mounting channel available. It is the same style of mounting channel that is used with MP metering products. It can be cut in the field to meet specific length requirements. The catalog number is EZM72MC.

CTA-ID : 14518
Was this helpful?
What can we do to improve the information ?