Technical FAQs

Ask a Question

What is the finish on the 9422A2 handle?

Side plates are stainless steel, all rivets are stainless steel and base is chrome plated die cast.


CTA-ID : 14142
Was this helpful?
What can we do to improve the information ?