Technical FAQs

Ask a Question

Which wire sizes are approved for the AL100FA4 lug for the FC and FCL breakers?

#14-#3 AWG Cu (2.5-35 mm2) Stranded Wire
#14-#8 AWG Cu (2.5-10 mm2) Solid Wire
#8-#1 AWG Al (10-50 mm2) Stranded Wire
#12-#10 AWG Al (2.5-6 mm2) Solid Wire


CTA-ID : 2035210
Was this helpful?
What can we do to improve the information ?