Technical FAQs

Ask a Question

Are the SG Magnet sensors waterproof?

Enclosure ratings NEMA 1, 4, 13.
Type 4 enclosures are intended for indoor or outdoor use primarily to provide a degree of protection against windblown dust and rain, splashing water and hose directed water...Please note that it is not corrosion resistant nor can it be submerged.


CTA-ID : 15990
Was this helpful?
What can we do to improve the information ?