Technical FAQs

Ask a Question

9007XA7309E and ...06E When plunger is depressed the contacts stick.<br />

There are two reason contacts might stick; 1 is the current is too high, 2. It`s too close to a magnetic field. Customer should test the magnetic field and the current

CTA-ID : 15986
Was this helpful?
What can we do to improve the information ?