Technical FAQs

Ask a Question

The MP44125 has 4 positions vertically on one side of the main lugs section. Was this device ever made with two positions on each side of the main lugs section?

An obsolete design, MP44125R, was made with the two positions on each side of the main lugs section. The MP44125R is no longer available.


CTA-ID : 2000352
Was this helpful?
What can we do to improve the information ?