Technical FAQs

Ask a Question

What type of material makes up the Class 8536 Type S NEMA 9 enclosures?

These enclosures are standard painted sheet steel with special super dust-tight gaskets.


CTA-ID : 14078
Was this helpful?
What can we do to improve the information ?