Technical FAQs

Ask a Question

How many AB1R* or AB1G* will fit on a given AB1 block ?

3 or 4 letter or number pieces will fit on each side depending on the block. The AB1SR6 can be mounted on the block to allow up to 6 letter or number pieces to be mounted on each side.

CTA-ID : 15963
Was this helpful?
What can we do to improve the information ?