Technical FAQs

Ask a Question

What is the deadfront part number for an NQOD424M100 or NQOD424M100CU interior?

Each panel will require the following:

(1) NQODRPL424BFMB1

Back-fed main breaker NQOD panels utilize a 1-pc deadfront. It covers the back-fed main as well as the branches.




CTA-ID : 2000331
Was this helpful?
What can we do to improve the information ?