Technical FAQs

Ask a Question

Is the 9007XA rated for an ambient temperature range of 0-350 degrees Farenheit?

Issue:
What is the limit switch that can be used from 0 to 350 degrees?

Product Line: 
Limit Switches

Environment:
North American Products

Cause:
​Would like to use the switch from 0 to 350 degrees Farenheit 

Resolution:

That temperature range is not a option for the 9007XA, the only option would be the HL switch on page 21-39 of digest 177
 
Was this helpful?
What can we do to improve the information ?