Technical FAQs

Ask a Question

What is the copper version of an HCWM12SN neutral?

A 80104-279-51 is a standard copper neutral w/AL lugs.
An HCWM12SNCU is a copper neutral w/CU lugs.


REJECTED: REFER TO FAQ 2002644



CTA-ID : 15724
Was this helpful?
What can we do to improve the information ?