Technical FAQs

Ask a Question

What is the part number for the copper version of an HCW4SN?

40517-426-51 (copper base w/ aluminum lugs)

HCW4SNCU (copper base w/ copper lugs)


Revised 4/27/04



CTA-ID : 15718
Was this helpful?
What can we do to improve the information ?