Technical FAQs

Ask a Question

Can you install a HOM240GFI or HOM250GFI breaker in a HOM24L70F load center?

When using a HOM GFI branch breaker, the HOM24L70F, S or RB has adequate wire bending space for a maximum #10 AWG wire. This will normally restrict the HOM GFI breaker to a maximum of 30 amperes.


CTA-ID : 15517
Was this helpful?
What can we do to improve the information ?