Technical FAQs

Ask a Question

Can the branch breakers QO240GFI, QO250GFI or QO260GFI be used in the QO24L70F / S / RB load centers?

Issue:
Product design features

Product Line:
QO Load centers

Environment:
Branch breakers

Cause:
Installation 

Resolution:

When using a QO-GFI branch breaker in the QO24L70F, S or RB, there is adequate wire bending space ONLY for a maximum #10 AWG wire. This will normally restrict the QO-GFI breaker to a maximum of 30 amperes.


CTA-ID : 15471
Was this helpful?
What can we do to improve the information ?