Technical FAQs

Ask a Question

Customer has been told the 9001 KY9 is obsolete. What is a good replacement for it?

Customer was advised the 9001 KYAF9 (priced the same as the KY9) or the 9001KYSS9 (more expensive than the KY9) could be used as replacements. However, the 9001KYAF has no Nema 4 rating. Also can use the 9001 KYAF12 and 3 hole plugs.

CTA-ID : 15366
Was this helpful?
What can we do to improve the information ?