Technical FAQs

Ask a Question

Can the QOM2200VH main breaker in a QO1816M200FTRB can be replaced with a QOM2150VH main breaker?

Issue:
Product Design features

Product Line:
QO load centers

Environment:
Main breaker

Cause:
Application

Resolution:
Yes, the main breaker can be replaced with any QOM2 frame main breaker up to 200 ampere maximum.


CTA-ID : 14822
Was this helpful?
What can we do to improve the information ?