Technical FAQs

Ask a Question

Can the HOM40L200C load center be converted to a Main Breaker device?

Product feature

Product Line:
Homeline Load Center

Clarification of product feature

It will depend on the Series number of the HOM40L200C. Series 1 and Series 2 were considered "fixed Main Lugs" and NOT convertible to Main Breaker. A Series S01 device may be converted to a Main Breaker by using a QOM2100VH (100 amp) through QOM2200VH (200 amp) Main Circuit Breaker Kit. A QOM2200VH would be the maximum Main Breaker allowed.

CTA-ID : 12249
Was this helpful?
What can we do to improve the information ?