Technical FAQs

Ask a Question

Can the power board be replaced on ATV16 drives?

Issue: Can the power board be replaced on ATV16 drives?
 
Product Line: ATV16
 
Environment: All
 
Cause: Powerboard replacement
 
Resolution: No. There are no replacement power boards available for the obsolete Altivar 16 drives. The drive should be replaced with a current product.

Reference resolution # 2003270 for crossreference information.


 
Was this helpful?
What can we do to improve the information ?