Technical FAQs

Ask a Question

What Tenant Circuit Breakers can be used with a EZMH112200 Meter Center?

This EZM Meter Center uses Q2M, Q2M-VH or Q2MH, 100 through 200 ampere, tenant circuit breakers. Example Catalog Number for 200 ampere - Q2M2200, Q2M2200VH or Q2MH2200. For 40 through 125 ampere requirements, the Q2M can be substituted with an EZM125QOA adapter and a QO, QO-VH or QOH, 40 ampere through 125 ampere, tenant circuit breakers. Example Catalog Number for 60 ampere - QO260, QO260VH or QOH260.


CTA-ID : 15923
Was this helpful?
What can we do to improve the information ?