Technical FAQs

Ask a Question

What is the part number for a NEMA 1 enclosure for the Class 8910 Type SYD*** definite purpose contactor?

8910SYD138 - 9991DPG5
8910SYD230 - 9991DPG6
8910SYD368 - 9991SGG8, This enclosure is supplied with an external reset mechanism. The mechanism can be removed and plugged with the 9001K51 closing plate.


CTA-ID : 2000281
Was this helpful?
What can we do to improve the information ?