Technical FAQs

Ask a Question

What are the lug sizes on the PBTB506G busway tap box?

There are two (2) lugs on each phase and neutral that will accept #2-500 kcmil wires. The ground lug will accept one #6-300 kcmil wire.

CTA-ID : 2000265
Was this helpful?
What can we do to improve the information ?