Technical FAQs

Ask a Question

Can customer use a lower rated fuse than what is specified in the spare parts list of bulletin VD0C06S304C?<br />

These fuses are selected for proper system coordination. These fuses are selected based on available fault current of 65KAIC. The customer can use a different fuse rated for lower current if they wish to do so or if their available fault current is less than 65K AIC

CTA-ID : 13163
Was this helpful?
What can we do to improve the information ?