Technical FAQs

Ask a Question

Are the UVR trip coils for the NSJ UL listed?

UL and CSA Listings for accessories

Product Line:
Circuit Protection:

Applies to NSJ accessories

UL and CSA listing for NSJ Undervoltage (UVR) accessory

Yes, the Undervoltage for the NSJ is UL listed.

Internal accessories comply with requirements of Underwriters Laboratories Inc.
UL 489 and Canadian Standard Association C22.2 No.5.1 Standards. All internal
accessories are Listed for fixed installation per UL file E103955 and Certified under
CSA file LR 69561.

CTA-ID : 9798
Was this helpful?
What can we do to improve the information ?