Technical FAQs

Ask a Question

Does the ATS46 have phase inversion protection?

Yes. It can detect phase rotation. It can be set to fault on phase reversal to prevent running the motor in the wrong direction. The normal direction can be either forward or reverse. There is also the option to have the PIF (inversion fault) turned off. The factory setting for PIf is off.

This also applies to enclosed Altistart 46 soft starters such as 8636, 8638, 8639


CTA-ID : 2000563
Was this helpful?
What can we do to improve the information ?