Technical FAQs

Ask a Question

What is the Electrical Interlock Kit for a DTU462, Series F5 double throw safety switch?

Use an EIK1 for 1 NO/1 NC contacts, EIK2 for 2 NO/2 NC. Two kits are required if the Electrical Interlock Kit is required for both operating positions.


CTA-ID : 2000560
Was this helpful?
What can we do to improve the information ?