Technical FAQs

Ask a Question

The 92452, rated 240Vac, has been replaced by the DTU462, rated 60Vac and 600Vdc. Is a 240Vac equivalent still availalbe?

The voltage ratings of the DTU462 are maximum values. The DTU462 can be applied at 240Vac. A 240Vac maximum rated device is not offered.

CTA-ID : 2000559
Was this helpful?
What can we do to improve the information ?