Technical FAQs

Ask a Question

Will the 9065TJF work on a 120/240V high leg system?

Yes, as long as there is very little current diference between phases. If there is considerable difference, suggest changing the overload relay to an LR3D----- type. This will eliminate the single phase sensitivity.

CTA-ID : 2000557
Was this helpful?
What can we do to improve the information ?