Technical FAQs

Ask a Question

Can an LC Main Breaker be used to series rate an NQOD Panelboard without remote mounting?

Yes, an LC breaker can be used to series rate in an NQOD panelboard without remote mounting. LC`s are available as integral main breakers on NQOD panelboards. (Ship fully assembled, factory assembled only.)

NOTE: The minimum box depth for this configuration is 8``.

Revised 3/10/04

CTA-ID : 2000554
Was this helpful?
What can we do to improve the information ?