Technical FAQs

Ask a Question

Can a HOM30M200RB load center be top fed?

Yes. The Main Breaker is located at the top of the interior. The incoming conductors can be fed from the top or bottom of the enclosure. The Main Breaker cannot be repositioned to the bottom of the interior.

CTA-ID : 2000547
Was this helpful?
What can we do to improve the information ?