Technical FAQs

Ask a Question

When using maintened signals with a ``T`` type motormechanism, do we need to disconnect B4 terminal ?

When using maintained signals with a ``T`` type motor mechanism, B4 terminal has to be connected. (disconnection of B4 only for the TS motor mechanism).


CTA-ID : 9718
Was this helpful?
What can we do to improve the information ?