Technical FAQs

Ask a Question

Are alternate lugs available for an H222NRB that will accept #1/0 AWG conductors?

No, the standard lugs of this switch will accept (1) #12 - 3 AWG Aluminum or (1) #14-3 Copper conductors per phase. There are no alternate lugs available for this switch.


CTA-ID : 2000540
Was this helpful?
What can we do to improve the information ?