Technical FAQs

Ask a Question

Can the HOM2200 Main breaker in the SC2040M200C be replaced with either a QOM2200 or QOM2200VH Service Disconnect?

Product design features

Product Line:
Combination Service Entrance Devices

The HOM2200 Main breaker CANNOT be replaced with a QOM2200 or QOM2200VH, it can ONLY be replaced with another HOM2200

CTA-ID : 2000537
Was this helpful?
What can we do to improve the information ?