Technical FAQs

Ask a Question

How does the9007 FT differ from the T limit switch?

The 9007FT is foundry duty switch and can withstand hot falling sand up to 300 degrees F. To accommodate the falling sand the FT longer shaft snout than the T.

CTA-ID : 2000538
Was this helpful?
What can we do to improve the information ?