Technical FAQs

Ask a Question

What is the part number for one-way screws for NF panel interior so that we can remove bus fingers and prevent them from being re-installed?

The screw is 21593-20100.


CTA-ID : 2000534
Was this helpful?
What can we do to improve the information ?