Technical FAQs

Ask a Question

What size wire can be used with Class 9080 GCB circuit protectors?

These circuit protectors are designed to accommodate quantity (1) #12 AWG conductor or quantity (2) #16 AWG conductors. (page 6 & 7 of 9080CT9301)


CTA-ID : 2000245
Was this helpful?
What can we do to improve the information ?