Technical FAQs

Ask a Question

Are the load lugs on Homeline branch breakers rated for both aluminum or copper conductors?

Yes. All Homeline breakers will accept copper or aluminum conductors on the load side lugs.


CTA-ID : 2035232
Was this helpful?
What can we do to improve the information ?