Technical FAQs

Ask a Question

What wire sizes may be used with the UL 489 listed C60 Multi 9 supplementary protector?

Connection, box lug:
0.5-25 A: #18-u#4 AWG (1-25 mm2) cables; torque 22 lb-in. (2.48 Nm)
30-35 A: #18-#2 AWG (1-35 mm2) cables; torque 31 lb-in. (3.52 Nm)


CTA-ID : 9579
Was this helpful?
What can we do to improve the information ?