Technical FAQs

Ask a Question

Can the In Phase Loss on the 8803 Omegapak be turned off?

This can only be done on the CT style units and is changed using the  Commissioning terminal (8803 PPO1 ) or PC software (no part number).

Go to the Special Functions menu and set the Phase fail. val. (Phase Failure Validation) to impliment the change.

Refer to instruction bulletin 50006-378-01A (June 1992) pages 107 or 138

CTA-ID : 4023
Was this helpful?
What can we do to improve the information ?