Technical FAQs

Ask a Question

How do I do 3-wire control with ATV28?

Issue:   How do I do 3-wire control with ATV28?
 
Product Line:  ATV28
   
Environment:  All
 
Cause:   N/A
 
Resolution:   In the I-O menu set the tCC parameter for 3C. LI1 will be the stop. LI2 will be forward. LI3 will become reverse. It is possible to change the setting for LI3 if desired.

 
Was this helpful?
What can we do to improve the information ?