Technical FAQs

Ask a Question

Do we supply the sealing rings on a ring type EZM meter sockets?

Yes, snap type aluminum sealing rings are provided. Optional sealing rings such as screw type aluminum and snap type stainless steel are also available..


CTA-ID : 2000219
Was this helpful?
What can we do to improve the information ?