Technical FAQs

Ask a Question

Can the operating handle of a LA400AWK circuit breaker enclosure be padlocked in the OFF position?

Issue:  
Need to lock the handle of the LA400AWK enclosure for LAL/LHL breaker ON. 

Product line:  
Circuit breaker enclosures

Environment:  
L-frame breaker NEMA 12/3R enclosure

Resolution:  
Yes, the external operating handle is provided with an integral lockplate for padlocking the handle in the OFF position.  
Was this helpful?
What can we do to improve the information ?