Technical FAQs

Ask a Question

What is the service bulletin part number of the Types MC30 ( PT-Mod H08; VT-Mod H07; part number 52011-548-53 {drive run relay}), MC31 (PT-Mod G08; VT-Mod G07; part number 52011-548-52 {non-isolated input}), MC32 (PT-Mod F08; VT-Mod F0 for the Omegapak 8804?

8804-52 is the part number of the manual.  
Web Link:

CTA-ID : 4202
Was this helpful?
What can we do to improve the information ?