Technical FAQs

Ask a Question

Merlin Gerin CM breaker with Shunt trip. Electrical interlocking.<br />Do the CM main contacts touch momentarily when the handle is moved to the<br />closed position while the shunt trip is energized? The breaker will trip<br />as the handle is moved to the on position, but will the main contacts touch<br />momentarily?

The Compact CM is ``kiss free``. The contacts do not touch.


CTA-ID : 1936
Was this helpful?
What can we do to improve the information ?